DEP settings

The DEP settings determine which applications and components are covered by DEP protection. They apply to both hardware-supported and software DEP features. On computers with the necessary hardware capabilities, hardware-supported DEP features are enabled for the same set of applications and components as the software DEP features. The following table explains the possible DEP settings and if they are supported by Rockwell Software products.
DEP Setting
Description
Supported by Rockwell Software Products?
AlwaysOn
Full DEP protection for the entire system (all applications and components, no exceptions).
No
OptIn (recommended)
DEP-enabled only for Windows system components and for applications that explicitly ”opt in."
Yes
OptOut
DEP-enabled for all processes except those that explicitly ”opt out."
Yes
AlwaysOff
DEP protection is disabled for the entire system (all applications and components, no exceptions).
Note:
Rockwell Software does not recommend using this setting, since it will make your system more vulnerable to malicious code.
Yes
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal