Upgrade an existing installation
You can upgrade an existing
RSLinx Classic
installation to version 4.60.00
(CPR 9 SR 16).
IMPORTANT:
The Installation Setup Wizard automatically backs up the driver configuration that exists
in the old version of
RSLinx Classic
, and restores the configuration
automatically into RSLinx Classic
version 4.60.00 (CPR 9 SR 16). You can
find the backup file BackupFromSystemInstall.rsx in
C:\Users\<username>\AppData\Local\Temp.To upgrade an existing installation:
- Close your current version ofRSLinx Classic.
- Insert theRSLinx ClassicDVD into the DVD-ROM drive. Refer toand perform the installation steps. The old version ofRSLinx ClassicGetting Results GuideRSLinx Classicthat exists on your computer is automatically uninstalled when you installRSLinx Classicversion 4.60.00 (CPR 9 SR 16).
- When the upgrade completes, restart your computer.
Provide Feedback