OPC UA Servers
- InFactoryTalk Administration ConsoleExplorer, right-click an OPC UA Connector, and then selectProperties.
- In, selectFactoryTalk LinxOPCUA ConnectorOPC UA Servers.
Use
OPC UA Servers
to configure settings and view the diagnostic information for each OPC
UA Server that communicates with a FactoryTalk Linx
OPC
UA Connector.OPC UA Servers
Lists the OPC UA Servers that the
FactoryTalk Linx
OPC
UA Connector is configured to communicate with. Status icons show the OPC UA Server status. Each connector supports up to 20 OPC UA Servers.Icon | Text | Description |
|---|---|---|
![]() | Communication is not started | The OPC UA Server configuration is not saved. The FactoryTalk Linx OPC UA Connector service is not attempting to connect to the OPC UA Server.To save the configuration and start the connection, select Apply or OK . |
![]() | Connecting with Server | The FactoryTalk Linx OPC UA Connector is attempting to connect to the OPC UA Server.Tip : If the FactoryTalk Linx OPC UA Connector stays in this state for an extended period of time, use the FactoryTalk Live Data Test Client to evaluate the "@OPC_Namespace…" predefined tags to monitor the namespace upload process. |
![]() | Disconnected with server | The FactoryTalk Linx OPC UA Connector cannot connect or has lost connection to the OPC UA Server. |
![]() | Uploading Namespace | The FactoryTalk Linx OPC UA Connector is uploading the OPC UA Server's namespace and presents the count of detected tags and the associated time cost for uploading. |
Communicating with server | The FactoryTalk Linx OPC UA Connector is connected to the OPC UA Server. |
Icon | Text | Description |
|---|---|---|
![]() | Communication is not started | The OPC UA Server configuration is not saved. The FactoryTalk Linx OPC UA Connector service is not attempting to connect to the OPC UA Server.To save the configuration and start the connection, select Apply or OK . |
![]() | Connecting with Server | The FactoryTalk Linx OPC UA Connector is attempting to connect to the OPC UA Server.Tip : If the FactoryTalk Linx OPC UA Connector stays in this state for an extended period of time, use the FactoryTalk Live Data Test Client to evaluate the "@OPC_Namespace…" predefined tags to monitor the namespace upload process. |
![]() | Disconnected with server | The FactoryTalk Linx OPC UA Connector cannot connect or has lost connection to the OPC UA Server. |
![]() | Listening for connection request | The FactoryTalk Linx OPC UA Connector is actively monitoring for incoming connection requests from the OPC UA Server. This status only applies to the case of a reverse connection. |
![]() | Server detected, retrieving endpoints | The FactoryTalk Linx OPC UA Connector has detected the OPC UA Server configured for reverse connection and is retrieving its endpoint URL to establish communication. |
![]() | Failed Connections: number | The FactoryTalk Linx OPC UA Connector fails to establish communication with the OPC UA Server through reverse connection and presents unsuccessful connection attempts for a duration of 10 seconds before switching the status to Listening for connection request . The failed connection count resets upon service restart or successful connection. Possible causes are as follows:
|
![]() | Uploading Namespace | The FactoryTalk Linx OPC UA Connector is uploading the OPC UA Server's namespace and presents the count of detected tags and the associated time cost for uploading. |
Communicating with server | The FactoryTalk Linx OPC UA Connector is connected to the OPC UA Server. |
Button | Description |
|---|---|
Add | Adds an OPC UA Server to the FactoryTalk Linx OPC UA Connector. |
Delete | Removes the selected OPC UA Server from the FactoryTalk Linx OPC UA Connector. |
UA Server Properties
Select a server from the
OPC UA Servers
list to view or edit its properties. Some properties have predefined diagnostic item counters that can be used for monitoring. If needed, use Reset Counters
command to reset diagnostic counter values to 0 for the server. Not all counters are resettable.Property | Predefined Diagnostic Item | Description |
|---|---|---|
Name | N/A | Sets the name for the OPC UA Server. The name must be unique. The server name displays in the FactoryTalk application tree and is included in the full tag path for all tags provided by the server. |
Description (optional) | N/A | Sets the description for the OPC UA Server as needed. |
Endpoint URL | N/A | Sets the network path to the OPC UA Server. The path must be in the format of opc.tcp:// where hostname_or_ip:port /EndpointName hostname_or_ip , port , and EndpointName are replaced with the host name or IP address, port number, and endpoint name of an OPC UA Server and its local discovery service.If no port is specified, the FactoryTalk Linx OPC UA Connector will attempt to connect to port 4880.The security system on the OPC UA Server must allow incoming connections to the selected port for the connection to succeed.If the OPC UA server is on the same computer as the connector, enter opc.tcp:// .localhost:port Typically, an OPC UA Server identifies its Endpoint URL within the server management interface. If the server or endpoint cannot be browsed, copy this URL from the server and enter it manually.If the UA Connector is configured to operate in a redundant configuration, one additional selection is available:
All the settings and configuration of OPC UA Servers are the same as the primary and secondary URLs. |
Reverse Connect | @OPC_ReverseConnectEnabled | Enables or disables the Reverse Connection function by selecting or clearing this checkbox. After this property is initially configured, any change to it requires restarting the FactoryTalk Linx OPC UA Connector service.The @OPC_ReverseConnectEnabled diagnostic item is read-only. |
Client Address | N/A | Specifies the host name or the IP address of FactoryTalk Linx OPC UA Connector.When the OPC UA Connector is configured locally, select the host name or IP address from the list or enter the value in the box. When the OPC UA Connector is configured remotely, the default is the host name. You can also choose to enter the IP address in the box. |
Client Port | N/A | Specifies the port of the OPC UA Client to be used for Reverse Connection. The port must not be used by another endpoint or application. Tip : FactoryTalk Linx OPC UA Connector will verify the usage availability of the specified port. When the OPC UA Connector is configured locally, the port that passes the verification is available to use. When the OPC UA Connector is configured remotely, you must go to the local workstation to verify if the port is used by another application. |
Client Endpoint URL | @OPC_ReverseConnectClientURL | Generates the network path to the FactoryTalk Linx OPC UA Connector in the format of opc.tcp:// based on the values specified in ClientAddress:ClientPort Client Address and Client Port . This value will be used by the OPC UA Server to initiate a reverse connection to the FactoryTalk Linx OPC UA Connector.This property is read-only. Select Copy next to this property to copy the value if needed. |
Server URI | @OPC_ReverseConnectServerUri | Displays the retrieved Server URI provided by the OPC UA Server. This property is read-only. |
Log Reverse Connect Server Uri | @OPC_ReverseConnectLogDiscoveredUrls | Determines whether to log the URL and URI for the reverse connected OPC UA Server to FactoryTalk Diagnostic Log . |
Property | Predefined Diagnostic Item | Description |
|---|---|---|
Security Policy | N/A | Determines what type of encryption algorithm is used for protecting data passed between the FactoryTalk Linx OPC UA Connector and the OPC UA Server.Use either:
|
Security Mode | N/A | Determines how the connection between the FactoryTalk Linx OPC UA Connector and the OPC UA Server is authenticated and whether the data is protected by encryption.Use either:
|
Certificate path | @OPC_CertificateOutgoingPath | Displays the path to the certificate provided by the FactoryTalk Linx OPC UA Connector. If the FactoryTalk Linx OPC UA Connector is hosted on a remote computer, the path represents the file location on the remote computer.The default path is C:\ProgramData\Rockwell\OpcUaConnector\RnaUaClientDataProvider\PKI\. |
Accept Incoming Certificate automatically | N/A | Allows the FactoryTalk Linx OPC UA Connector to accept the certificate of OPC UA Server automatically. This checkbox is selected by default and cannot be cleared. |
Property | Predefined Diagnostic Item | Description |
|---|---|---|
Anonymous | N/A | Uses an anonymous connection to the OPC UA Server |
User name & Password | N/A | Specify the user name and password to use to log on to the OPC UA Server. |
Property | Predefined Diagnostic Item | Description |
|---|---|---|
Tag update rate override | @DAQ_ScanRateOverrideActive | Determines the update rate for each UA server that the FactoryTalk Linx OPC UA Connector uses to request a tag.
|
Array access method | N/A | Determines how the FactoryTalk Linx OPC UA Connector accesses data on the UA Server.
|
Permit value writes to array elements | N/A | Selects this option to enable writing to arrays. This option works with the array access method to control writing data to the array. When using the default array access method - Operate on entire array at once (all elements) - selecting this option results in writing the entire array if an element within the array changes. The array is read into memory, the elements that were modified are changed, and then the array is written back to the OPC UA server. There is a potential that the data on the OPC UA Server changed after it was read. These changes will be overwritten by the previously read data, which could lead to some data inconsistencies.If the UA Server supports indexed arrays, selecting the Access subset of array (indexed elements) access method and then enabling this option results in writing only changed elements within an array. Before using this mode in a production system, test the results to confirm that the values are updating as expected. |
Unsupported types | N/A | Selects Provide string tags for unsupported types to convert the OPC UA Connector data types that are not supported in Live Data to strings. |
Monitor Item Mode | @OPC_MonitorItemTriggerMode | Selects FactoryTalk Linx OPC UA Connector the source timestamp to be delivered with each tag value it receives and passes to a FactoryTalk Live Data client when the source timestamp changes.
|
Property | Predefined Diagnostic Item | Description |
|---|---|---|
Enable alarm and event support | N/A | Enables alarm and event support and activate the options on the properties dialog box by selecting the checkbox. By default, this setting is disabled. |
Status icon | @OPC_AlarmEventProviderStatus | Shows the alarm server status.
|
Priorities | N/A | Used to enable group alarm severities. Grouping severities by priority level helps operators filter and sort alarms more quickly and distinguish among degrees of urgency. Select the Enable server-assigned priorities checkbox to override default system-wide priority settings with FactoryTalk Linx OPC UA server-specific priorities.The following are the default server-assigned priorities and their associated default severity range:
|
Enable history | N/A | By default, this setting is disabled. When the setting is disabled, you can view the alarms, but the alarms will not be recorded. |
Database definition | N/A | Used to select a database definition that receives data from the alarm server. Tip: If you have not created a database definition, refer to FactoryTalk Alarms and Events Help |
Computer Name | N/A | Displays the name of the computer that contains the database. |
Database name | N/A | Displays the name of the database to which the data is logged. |
Cache file path | N/A | Displays the location of alarm and event data cache files. If the connection to a database is lost, alarm and event history is cached to files in this path. Once the connection to the database is restored, the information in the cache files is written to the database. Only change the default value if the location does not have enough free disk space. The cache file location must be local to the computer hosting the alarm server so that events can be cached if the computer is temporarily disconnected from the network. |
Property | Predefined Diagnostic Item | Description |
|---|---|---|
Log diagnostic message on tag write | N/A | Enable this item to include events related to writing data to tag values in the diagnostic log. |
Property | Predefined Diagnostic Item | Description |
|---|---|---|
Last Refreshed | @OPC_NamespaceCacheLastRefreshedDateMsg | Displays the most recent date and time that the FactoryTalk Linx OPC UA Connector refreshed the namespace cache of the specified OPC UA Server. |
Refresh Tag Names | @OPC_NamespaceCacheUploadCmd | Updates all tag information sent from the OPC UA Server. |
Analyze Tag Names | @OPC_NamespaceAnalysisCmd | Analyzes the namespace of the OPC UA server and saves a report of all namespace items that have unsupported data types.The FactoryTalk Linx OPC UA Connector saves the namespace on its host computer to the file C:\ProgramData\Rockwell\OpcUaConnector\RnaUaClientDataProvider\AddressSpace\ConnectorName_ServerName_ServerEndpointURL.txt . In the output filename, ConnectorName, ServerName, and ServerEndpointURL are replaced with the names and Endpoint URL of a FactoryTalk Linx OPC UA Connector and OPC UA Server configured in FactoryTalk Linx OPC UA Servers > OPC UA Servers |
Property | Predefined Diagnostic Item | Description |
|---|---|---|
Monitored Tags | @OPC_ItemsMonitoredQty | The number of tags in all subscriptions that FactoryTalk Services Platform monitors for data from the OPC UA Server. |
Bad Quality Tags | @OPC_ItemsBadQualityQty | The number of tags with Bad quality provided by an OPC UA Server. |
Tag Updates / Second | @OPC_ItemsUpdatedRate | The rate in tag values per second at which the OPC UA Server sends tag values to the FactoryTalk Linx OPC UA Connector. |
Requested Groups | @OPC_SubscriptionQty | The number of subscriptions to the OPC UA Server. |
Failed Item Requests | @OPC_CommSubscriptionsFailedQty | The number of subscriptions that entered an error state for an OPC UA Server. |
Property | Predefined Diagnostic Item | Description |
|---|---|---|
Attempted Tag Writes | @OPC_ItemsWrittenQty | The number of attempted writes to tags in an OPC UA Server. |
Failed Tag Writes | @OPC_ItemsWrittenErrorsQty | The number of tags write errors logged by an OPC UA Server. |
Property | Predefined Diagnostic Item | Description |
|---|---|---|
Write with Timestamp Supported | @OPC_SessionSupportsTimestampsOnWritesStatus | Whether the OPC UA Server supports writing values with time stamps. Defaults to True until the server rejects writing a value with a time stamp. |
Tags Detected | @OPC_NamespaceTotalTagsInServerQty | The number of OPC UA items in the OPC UA Server that have supported data types and are converted to FactoryTalk tags. |
Node IDs Detected | @OPC_NamespaceTotalNodesInServerQty | The number of OPC UA items in the OPC UA Server. |
Performance Reads/Second | @OPC_ServerPerformanceReadRate | A performance rating of an OPC UA Server, based on the amount of time required to read a node. |
Performance Writes/Second | @OPC_ServerPerformanceWriteRate | A performance rating of an OPC UA Server, based on the amount of time required to write a node. |
Sessions | @OPC_CommConnectionQty | The number of active sessions for an OPC UA Server. Increments by one when a session connection succeeds. Decrements by one when a session connection fails. |
Communications Errors | @OPC_CommConnectionFailedQty | The number of communication errors reported from the OPC UA Server. |
Longest Processing Time (msec.) | @OPCtoDAQ_LongestTimeProcessingData_mSec | The longest amount of time in milliseconds that an OPC UA Server spent processing data. |
Alarms Detected | @OPC_AlarmTotalAlarmConditionsQty | The number of alarms detected. |
Alarms Bad Quality | @OPC_AlarmFaultedAlarmConditionsQty | The number of alarms with bad quality condition. |
Alarms Active | @OPC_AlarmActiveAlarmConditionsQty | The number of active alarms. |
Alarms Disabled | @OPC_AlarmDisabledAlarmConditionsQty | The number of alarms disabled. Disabling an alarm prevents the operator from being notified when the alarm condition occurs. |
Alarms Acknowledged | @OPC_AlarmAckedAlarmConditionsQty | The number of alarms acknowledged. Acknowledging (Ack) an alarm does not correct the condition causing the alarm-it indicates that an operator is aware of the alarm. |
Alarms Suppressed | @OPC_AlarmSuppressedAlarmConditionsQty | The number of alarms suppressed. Suppress an alarm that is not needed temporarily. |
Alarms Shelved | @OPC_AlarmShelvedAlarmConditionsQty | The number of alarms shelved. Shelving an alarm temporarily suppresses it. |
Property | Predefined Diagnostic Item | Description |
|---|---|---|
Tag Requests | @DAQ_ItemsAddedQty | The number of tags that FactoryTalk clients request from the OPC UA Server. |
Failed Tag Requests | @DAQ_ItemsAddFailureQty | The number of tags that FactoryTalk clients request, but do not exist in the OPC UA Server. |
Active Tags | @DAQ_ItemsActiveQty | The number of tags in the active state that FactoryTalk clients request from the OPC UA Server. |
Inactive Tags | @DAQ_ItemsInactiveQty | The number of tags in the inactive state that FactoryTalk clients request from the OPC UA Server. |
Tag Updates / Second | @DAQ_TagsUpdatedRate | The rate in seconds at which the OPC UA server sends updated values to Live Data tags |
Property | Predefined Diagnostic Item | Description |
|---|---|---|
Reset Counters | @DP_CounterResetCmd | Resets all resettable diagnostic counters for this OPC UA Server. Does not affect any other OPC UA Server. |
Provide Feedback