Regenerate the certificate
When an OPC UA Connector begins communication with an OPC UA Server, the OPC UA Connector provides the OPC UA Server with its security certificate. The OPC UA Server accepts or rejects the certificate to authorize or deny communication to the OPC UA Connector. Security certificates may be required for some OPC UA Servers.
FactoryTalk Services Platform
creates a default, self-signed security certificate during installation. The certificate is stored at C:\ProgramData\Rockwell\OpcUaConnector\RnaUaClientDataProvider\PKI\own\
on the computer hosting FactoryTalk Linx
OPC UA Connector. If a security certificate signed by a trusted security authority is required, replace the default security certificate with the required certificate. A custom security certificate must have the same name and file path as the default security certificate.
FactoryTalk Linx
OPC
UA Connector version 6.20.00 or later supports creating a Certificate Signing Request (CSR) to obtain a new certificate from an external signing authority.
TIP:
Use
Manage Access
to limit access to security certificate management operations to administrators or individuals. This function is only available to Administrator.To regenerate the FactoryTalk Linx OPC UA Connector certificate
- InFactoryTalk Linx OPC UA Connector, selectCertificate Management.
- OnCertificate Management, selectOutgoing Certificate, and then selectRegenerate.
- InRegenerate Certificate, enter your password twice inPasswordandConfirm, and then selectContinue.TIP:TheRestart FactoryTalk Linx OPC UA Connector servicecheckbox is selected by default. For more information about this checkbox, see Regenerate Certificate.
Provide Feedback