Remove an OPC UA Server

Remove an OPC UA Server from an OPC UA Connector to remove tags from
FactoryTalk
applications.

Prerequisites

  • Obtain the following permissions for the application or area in
    Explorer
    :
    • Common > List Children
    • Common > Read
    • Common > Delete

To remove an OPC UA Server from an OPC UA Connector

  1. In , select
    OPC UA Servers
    .
  2. On
    OPC UA Servers
    , select an OPC UA Server, and then select
    Delete
    .
  3. Select
    Apply
    .
  4. In , select
    Yes
    .
    IMPORTANT:
    FactoryTalk
    clients do not receive OPC UA tags from any OPC UA Servers connected to this OPC UA Connector until the reset is complete.
  5. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal