Register device description files
You can register the device description files of hardware devices, including EDS and IODD files, by launching the
Device Description File Installation Tool
.Before you begin to register the device description file of a hardware device, you must have a valid and complete device description file of the hardware device. To search and download the device description file of a specific hardware device, visit Rockwell Automation Network Resources. In addition, if an icon file (*.ico) exists for the hardware device, save it with the same name as the device description file in the same directory. You can save one or more device description files (and the related icon files) in one directory.
To register device description files of hardware devices
- Launch the Device Description File Installation Tool fromStart > Rockwell Software > Device Description File Installation Tool.
- In theRockwell Automation - Device Description File Installation Tooldialog box, selectAdd.TheDevice Description File Installation Tooldialog box opens.
- On theRegistrationscreen, selectRegister a single device description fileto register one device description file at a time, orRegister a directory of device description filesto register two or more device description files at a time. Then clickBrowseto select the device description file (if you are registering a single file), or the directory of the device description files (if you are registering two or more files), and clickNext.
- On theDevice Description File Installation Test Resultsscreen, review the hardware device list, and clickNext.
- On theChange Graphic Imagescreen, review the icon(s) of the hardware device(s), and clickNext.TIP:Device Description File Installation Tool assigns a default icon to each hardware device. You can specify another icon for the hardware device(s) by selecting the hardware device and clicking theChange iconbutton.
- On theFinal Task summaryscreen, review the hardware device list and clickNext.
- When the registration is complete, clickFinishto return to theRockwell Automation - Device Description File Installation Tooldialog box.
- ClickExit.
Provide Feedback