About the virtual backplane

The virtual backplane is a driver service that provides connectivity between
FactoryTalk Linx
and various device drivers and other applications within the
FactoryTalk Linx
server using the CIP protocol. It allows the software modules and communications resources contained in the server to be configured and visualized in a manner similar to the devices in a
ControlLogix
system. Once USB CIP devices are added to the virtual backplane, FactoryTalk Linx will automatically mirror the devices into the USB branch in the topology tree.
For example, both the PCICS and PKTCS device drivers plug into the virtual backplane. Packets received by one of these communications interface cards can be routed across the virtual backplane to (or through) any other interface card whose driver plugs into the virtual backplane, or to any application that plugs into the virtual backplane, such as the
SoftLogix
5xxx controller.
This is similar to having a 1756-CNB and a 1756-ENBT module plugged into a
ControlLogix
chassis: packets received across the ENBT can be routed across the backplane out the CNB module, or to a controller sitting in the backplane.
Note that
RSLinx Classic
occupies slot 0 and that
FactoryTalk Linx
occupies slot 1 in the virtual backplane, which means that they are able to be both a source and a destination for packets sent over the backplane.
This chassis-like model is carried over to the
PanelView Plus
platforms in a minimalist fashion. For ControlNet support, those platforms implement two-slot virtual backplanes, where
FactoryTalk Linx
sits in one slot and the 2711P-RN15S ControlNet Scanner card sits in the other.
TIP:
When you select the virtual backplane on the user interface,
FactoryTalk Linx
may not automatically discover the devices that reside in it. This is most likely to happen if you have added the device with a separate software package such as the
SoftLogix
Chassis Monitor or
RSLinx Classic
.
If you think you have devices resident in your virtual backplane that are not showing up on the
FactoryTalk Linx
user interface, right-click the virtual backplane and select
Start Browsing
or
Show All Devices
to see those devices. Note that saved configuration data is not lost if the devices do not appear.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal