Using graphic objects

To monitor alarms at runtime,
FactoryTalk Alarms and Events
provides these graphic objects used to view and interact with alarm conditions:
  • Alarm and Event Summary
  • Alarm and Event Banner
  • Alarm Status Explorer
FactoryTalk Alarms and Events
provides an object with which to view and run reports on historical alarms:
  • Alarm and Event Log Viewer
To use these objects, insert them into
FactoryTalk View
graphic displays.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal