Set up graphic displays
Graphic displays created in
FactoryTalk View Studio
are containers for FactoryTalk Alarms and Events
objects, such as the Alarm and Event Summary object. FactoryTalk Alarms and Events
objects are used to monitor and interact with device-based, tag-based, and OPC UA alarms at runtime.Add alarm and event objects to
FactoryTalk View
graphic displays- RunFactoryTalk View Studioand open an existing application.
- Expand theFactoryTalkExplorer window to display the HMI Server where you want to add the new graphic display.
- If the application does not yet have an HMI Server, add one. Right-click the application or area, point toAdd New Server, and then clickHMI Server. Follow the instructions on the HMI Server Wizard.You can only add HMI servers to a View SEnetwork distributedapplication. Bothnetwork stationapplications andlocal stationapplications support a single HMI server, which is provisioned silently by the system when the application is created.
- In theGraphicsfolder, right-clickDisplays, and then clickNew.
- On the menu bar, click onObjects, point toAlarm and Event, and then click one of the objects listed:Banner,Summary,Log Viewer,Status Explorer,orAutomatic Diagnostic Event Summary.
- Click in the grid and drag the cursor to position and size the object on the graphic display.
- Double-click the object to configure its properties.For step-by-step instructions, see the, available from theFactoryTalk Alarms and EventsSystem Configuration GuideHelp > Online Booksmenu inFactoryTalk View Studio.
- When you finish, clickOKto close the object properties, and then clickFile > Saveto save the graphic display.
- Create additional graphic displays and insert and configure other Alarm and Event objects as needed.
Provide Feedback