Redundant device-based alarm servers

What you need:
  • FactoryTalk Linx
    and
    FactoryTalk Alarms and Events
    installed and running on the primary server computer--configured and working as a non-redundant component.
  • FactoryTalk Linx
    and
    FactoryTalk Alarms and Events
    installed and running on the secondary server computer.
  • FactoryTalk View Studio
    or
    FactoryTalk Administration Console
    running on a development station or on another connected component in the application.
To set up redundancy for device-based alarm servers:
  1. Set up device-based alarm monitoring.
  2. Configure a device-based alarm server to support redundancy using the configured secondary computer.
  3. Check the status of the alarm server.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal