Select FactoryTalk Directory
How do I open Select
FactoryTalk Directory
?
- Close and re-openFactoryTalk Administration Console.Selectopens whenFactoryTalk DirectoryFactoryTalk Administration Consolestarts.
Use
Select
to log into a FactoryTalk Directory
FactoryTalk Directory
. Select the FactoryTalk Directory
type that corresponds with the FactoryTalk
system.Option | Description |
|---|---|
Network | Select to work with network applications that are distributed across a network. A network application organizes project information from multiple FactoryTalk products and services distributed across multiple computers on a network. |
Local | Select to work with local applications that are constrained to this local computer. All local application components and participating software products are located on this local computer. |
Provide Feedback