Backup
How do I open Backup?
In the
Explorer
window, right-click the directory icon, an application, or the System
folder, then click Backup
.Use
Backup
to specify:- The name and location of a backup file
- Whether or not to include the System folder in the backup (application backup only)
- Whether or not to encrypt the backup archive
- A passphrase for the encrypted archive, if usedSettingDescriptionSpecify archive nameUse the default archive name or type a name for the archive file. The extension .bak is added automatically. You do not have to type it.
- By default, an archive file that contains a backup of an entireFactoryTalk Directory(including all applications, all user and computer accounts and groups, passwords, policy settings, and security settings) is named with its current security authority identifier, for example,Network - 72CE2C2E-5175-4C26-98AE-3ABE5AC7F8EC.bakorLocal - C565C77A-4664-4E6C-9779-1EC729B3A8A0.bak. It is recommended that you do not change the default archive name. The default name contains the leading digits of the security authority identifier, which allows you to easily identify the archive file associated with a specific directory.
- By default, an archive file that contains a backup of a System folder (including user and computer accounts and groups, passwords, policy settings, and security settings) is namedSystem.bak.
- By default, an archive file that contains a backup of a single application is named the same as the application. If you are backing up an application, you can optionally also include the contents of the System folder in the backup archive.
Specify archive locationUse the default archive location or type the path where you want to save the backup file. Alternatively, selectBrowse,select a folder, and selectOK.The default archive location isC:\Users\Public\Documents.FactoryTalk Directory configurationSelect this option to back up the entireFactoryTalk Directory.IMPORTANT: The archive file does not contain project files that are specific to individual products.The archive file includes:- All objects, references to objects held within theFactoryTalk Directory, and the security authority identifier. The archive file does not contain project files that are specific to individual products.
- All applications associated with that directory. Typically an application contains areas (in a network directory), resource grouping information, and references to data servers, device servers, alarm servers, and HMI servers.
- The System folder, which includes a list of user, computer, and group accounts, passwords, system policy settings, product policy settings, system security settings, action groups, and alarm and event database definitions.
- FactoryTalk LinxOPC UA Connector configurations for all computers configured in the directory.
FactoryTalk Linx configurationSelects this option to back up allFactoryTalk Linxshortcut configurations and associated paths. The configuration file does not contain CIP security information.The backup operation can only save the FactoryTalk Linx drivers and shortcuts configured on this workstation.Refer to BackupFactoryTalk Linxconfiguration to find how to backup a distributed system. Refer to RestoreFactoryTalk Linxconfiguration to find how to restore a distributed system.Selects this option to back up server configuration, UA Server Endpoint settings, Advanced Settings, and UA Tag List configuration inFactoryTalk Linx Gateway.System Directory configurationTheSystem Directory configurationbox is checked by default when you are backing up the System folder.Moreover, it is available if you are backing up an application.- To include the contents of the System folder in the backup archive, select this check box.
- Choose this option when you want to restore only one application from aFactoryTalk Directory, but want to include all user and computer accounts and groups, passwords, policy settings, and security settings from the originalFactoryTalk Directory.
- To back up only the application without the System folder, clear this check box.
- Choose this option when you want to add an application to an existingFactoryTalk Directorywithout overwriting the settings held in the System folder.
Application Directory configurationThe Application Directory configuration box is checked by default when you are backing up the selected application.The application data server settings and theFactoryTalk LinxOPC UA Connector configuration for all computers configured in the application will be saved.File EncryptionChoose whether or not to encrypt the archive file. Encrypting the file protects it against unauthorized use.The check box will not be available if your operating system does not support the proper level of encryption. To use the file encryption, install yourFactoryTalksoftware on one of the supported operating systems.- To encrypt file contents, select theFile Encryptioncheck box.
- To save the archive file without encryption, clear this check box.
PassphraseType a passphrase for the archive file you want to encrypt.The passphrase must meet the following requirements:- Any alphanumeric character or other characters
- Minimum length: 0
- Maximum length: 64
Confirm passphraseType the same passphrase you typed in thePassphrasefield.
IMPORTANT:
Remember the passphrase if you choose to encrypt your file contents. The archive file cannot be restored without the correct passphrase.
FactoryTalk Services Platform
6.10 applies a new encryption algorithm to the backup file for enhanced security. Backups created using FactoryTalk Services Platform
6.10 can only be restored to host computers that are also running FactoryTalk Services Platform
6.10 or later. Backups created using FactoryTalk Services Platform
2.90 or later can be restored onto host computers that are running FactoryTalk Services Platform
6.10.Provide Feedback