Back up an application
An application typically contains areas (in a network directory), resource grouping information, and references to data servers, device servers, alarm servers, and HMI servers.
Back up an application and create an archive file to:
- Restore the application to aFactoryTalk Directoryon a different computer
- Duplicate the application with a different name within the same directory
Optionally, include the System folder in the archive. The System folder includes a list of user, computer, and group accounts, passwords, system policy settings, product policy settings, system security settings, action groups, and alarm and event database definitions. Refer to Restore an application to find the steps to restore an application.
Prerequisites
- Obtain the security permissions needed to perform backup and restore operations. OpenSystem > Policies > System Policies, and double-clickUser Rights Assignment.
To back up an application
- InFactoryTalk Administration ConsoleExplorer, right-click the selected application, and selectBackup.
- Use the default name or enter another name for the backup file.
- Use the default archive location or specify another location by selectingBrowse, selecting a location, and then selectingOKin theBrowse for Folderwindow.
- In Backup Contents:
- To exclude theSystemfolder in the backup, clear theSystem Directory configurationcheck box. To include the System folder in the backup, select theSystem Directory configurationcheck box.TIP:You can still choose to restore only the application from the backup archive file later, even if you include the System folder in the backup.
- (optional) Selectto back up shortcut and driver configurations.FactoryTalk Linxconfiguration
- (optional) Selectto back up server configuration, UA Server Endpoint settings, Advanced Settings, and UA Tag List configuration inFactoryTalk Linx GatewayconfigurationFactoryTalk Linx Gateway.
- To encrypt your archive file, select theEncrypt file contentscheck box, and then enter the same passphrase in thePassphraseandConfirm passphrasefields. If you clear this check box, your backup archive file will not be encrypted or protected.TheEncrypt file contentscheck box will not be available if your operating system does not support the proper level of encryption.IMPORTANT:Remember the passphrase if you choose to encrypt your file contents. The archive file cannot be restored without the correct passphrase.
- In theBackupwindow, selectOK.Unless you specified a different file name,FactoryTalkAdministration creates anApplicationName.bakfile for the application in the default location, or in the location you specified. If a backup file with the same name already exists in the location you've chosen, the system asks whether you want to overwrite the existing file.After backing up an application, back up and restore project files and databases separately from individual software products that are participating in theFactoryTalksystem.If your applications include:
- HMI servers, back up and restoreFactoryTalk Viewfiles separately. SeeFactoryTalk Viewdocumentation for help.HMI servers:Back upFactoryTalk Viewfiles separately. SeeFactoryTalk Viewdocumentation for help.
- Run theRSLinx Classicdata servers:RSLinxBackup Restore utility to back up the data server configuration. From themenu, selectWindowsStartRockwell Software >.RSLinx> Backup Restore Utility
- The base configuration of theFactoryTalk Linxservers:FactoryTalk Linxserver is included in the backup, including redundancy and alarms and events configurations.TIP:If theFactoryTalk Linxconfiguration option is not selected, make a copy of the fileRSLinxNG.xmland keep it with your backup archive to retain device, driver, and shortcut configurations. By default, the file is located inC:\ProgramData\Rockwell\RSLinxEnterprise.
- : OpenFactoryTalk LinxData BridgeFactoryTalk LinxData Bridge, selectFile > Export configuration. Keep the exported file with your backup archive.
- :FactoryTalk LinxGateway
- ForFactoryTalk LinxGateway version 6.20 and earlier, make a copy of theFTLinxGateway.xmlfile and keep it with your backup archive. By default, the file is located inC:\ProgramData\Rockwell\FactoryTalk Linx Gateway.
- ForFactoryTalk LinxGateway version 6.21, make a copy of theFTLinxGateway.dbfile and keep it with your backup archive. By default, the file is located inC:\ProgramData\Rockwell\FactoryTalk Linx Gateway.TIP:If there are two files named asFTLinxGateway.db-shmandFTLinxGateway.db-walunder the folderC:\ProgramData\Rockwell\FactoryTalk Linx Gateway, make a copy of these two files together withFTLinxGateway.dbfile.
- : The base configuration for the OPC UA Connector can be restored. After the restore operation is completed, you will need to regenerate a certificate and enter a password to return the OPC UA Connector to full operation.FactoryTalk LinxOPCUA Connectors
- Use MicrosoftFactoryTalk Alarms and EventsLogs:SQL Servertools to back up and restore database files.
- : Back up project files using theFactoryTalk Transaction ManagerConfigurationmenu. SeeFactoryTalk Transaction Managerdocumentation for help.
- Copy theFactoryTalk Batch:FactoryTalk Batchfiles back to the same directory locations. SeeFactoryTalk Batchdocumentation for help.
- Other products: Back up product-specific information separately. See product documentation for help.IMPORTANT:FactoryTalk Services Platform6.10 applies a new encryption algorithm to the backup file for enhanced security. Backups created usingFactoryTalk Services Platform6.10 can only be restored to host computers that are also runningFactoryTalk Services Platform6.10 or later. Backups created usingFactoryTalk Services Platform2.90 or later can be restored onto host computers that are runningFactoryTalk Services Platform6.10.
Provide Feedback