Reset FactoryTalk Linx Gateway
When you cannot open or save the configurations or want to start with a new / empty configuration, the following process can be used to reset FactoryTalk Linx Gateway. This will create a new configuration similar to the default one after installation. If you want to use a previous configuration, perform a backup and restore operation:
Prerequisites
- Make sure that the system or environment will not be impacted.
- Make sure that you have administrator rights.
To reset FactoryTalk Linx Gateway
- Close FactoryTalk Linx Gateway Configuration.
- Go to WindowsServices, and then stop these FactoryTalk Linx Gateway services:
- FactoryTalk Linx Gateway Administration Service
- FactoryTalk Linx Gateway Configuration UI Service
- FactoryTalk Linx Gateway OPC DA Server
- FactoryTalk Linx Gateway OPC DA Standalone Server
- FactoryTalk Linx Gateway OPC UA Server
- FactoryTalk Linx Gateway Supervisor
- Go to C:\ProgramData\Rockwell, and then delete theFactoryTalk Linx Gatewayfolder.
- Restart FactoryTalk Linx Gateway.
Provide Feedback