FactoryTalk Linx Gateway's OPC UA service does not appear in the OPC Local Discovery Service (LDS)
Possible causes and solutions
- FactoryTalk Linx Gatewayis not configured
- No data sourceTo solve this issue, configure the related data source based on the activation type and apply the system configuration.
- OPC UA is disabledTo solve this issue, enable the OPC UA server onGlobal Settings.
- No endpoint configuredTo solve this issue, configure the endpoint URL onEndpointsand apply the system configurations.
- An endpoint is disabledTo solve this issue, enable the endpoint.
- FactoryTalk Linx GatewayOPCUA service is not startedTo solve this issue, start the OPC UA service fromControl Panel > System and Security > Administrative Tools > Services >FactoryTalk Linx Gateway.OPCUA Server
- FactoryTalk Linx GatewayOPCUA service is disabledTo solve this issue, enable the OPC UA server onGlobal Settings.
- FactoryTalk Linx Gatewayis not activated correctly or activation is expiredTo solve this issue, get a new key from Rockwell Automation.
- The option to register with the LDS is disabledTo solve this issue, selectRegister with Discovery ServiceonUA Server Interface.
- FactoryTalk Linx Gatewayhas not trusted the OPC LDS certificateTo solve this issue, selectTrustonIncoming Certificateto add the LDS certificate into the trust list.
- The OPC LDS certificate has expiredTo solve this issue, stop the service and delete its certificate from the hard drive. Once the service starts it will automatically regenerate the certificate.
- OPC Local Discovery Service (LDS) service is not startedTo solve this issue, start the LDS service fromControl Panel > System and Security > Administrative Tools > Services > OPC UA Local Discovery Server.
Provide Feedback