Slow or unreliable communications
Possible cause and solution:
- TheFactoryTalk Linx Gatewayhost computer is out of memory or out of disk spaceEnsure theFactoryTalk Linx Gatewayhost computer meets the System requirements inFactoryTalk Linx GatewayRelease Notes.
- TheFactoryTalk Linx Gatewayhost computer is at maximum CPU load.Ensure theFactoryTalk Linx Gatewayhost computer meets the System requirements inFactoryTalk Linx GatewayRelease Notes.Change anti-virus scan settings to only run during off-peakFactoryTalk Linx Gatewaycommunication periods.Move other services on theFactoryTalk Linx Gatewaymachine to a new host computer until the runtime load is reduced.Rockwell Automationrecommends a 40% maximum steady state CPU load. This balances utilization of the hardware and provides enough bandwidth for peak loads.
- A firewall or switch is blocking some or allFactoryTalk Linx Gatewaycommunications.Verify firewall and switch rules allowFactoryTalk Linx Gatewaycommunications. For a list of ports used byFactoryTalk Linx Gateway, see Application notes inFactoryTalk Linx GatewayRelease Notes.
- TheFactoryTalk Linx GatewayCPU usage is highReduce the number of clients packaging data to OPC standards.Limit the number of clients requesting data from a single OPC data server.Restrict the action of changing groups by clients.
- The network is not configured correctly.Check your network configuration andFactoryTalk Linx Gatewayinstallation.
- The controller CPU usage is too high.Use Logix Designer Task Monitor to monitor task utilization and take proper actions.
- The communication efficiency linked to Ethernet Module is low.ENET, ENBT, EN2T, or EWEB modules could be a bottleneck to communications depending on the number of data requests and the number of requesting clients.
- The communication efficiency is affected by tag structure.Seeonline help.Studio 5000 Logix Designer
- The communication efficiency is affected by the time slice setting.Increase the time slice value in Logix Designer application.
- The ControlLogix Optimized Packets process is hindered.Refer to your ControlLogix controller documentation.
- OPCUA or DA service is stopped.Check the Server Configuration tab, make sure the UA and DA Server is not disabled. Or go to windows Services tool to restart theOPCUA or DA service.
- A hard-coded 6-minute time-out notification received.Verify the server and client connection, both physical and software level.
- A reboot is required forOPCservers and client.Verify theOPCserver and client are successfully reconnected to the original objects after disconnection.
Provide Feedback