Naming conventions in Custom RTD Namespace
The following table shows the naming conventions in
Custom RTD Namespace
.Type | Limitation | Maximum length | Case-sensitive (Yes or No) |
|---|---|---|---|
Tag name* | The name must consist of any character from the following:
| 256 | No |
Tag descriptions | The descriptions cannot contain quotation marks. | 256 | N/A |
*Upper and Lower case letters in names are helpful for presentation only. Names are not case-sensitive.
Provide Feedback