Develop software to interface with FactoryTalk Linx Gateway
You can develop your own client to interface with
FactoryTalk Linx Gateway
OPC
UA, MQTT, OPC DA, DDE, and Linx SDK. We recommend acquiring an OPC
client toolkit from the OPC
Foundation and developing custom source code using the standard toolkit for OPC UA and OPC DA.Provide Feedback