Back up FactoryTalk Linx Gateway configuration
FactoryTalk Services Platform
provides an option to back up FactoryTalk Linx Gateway
configuration configured on the same computer. You can back up the current settings and
restore them later to control the settings, especially when the application or scope (Local
or Network) of FactoryTalk Linx
is changed.
IMPORTANT:
- During a backup operation, some FactoryTalk services will be temporarily locked, preventing new requests from being processed. This situation will result in new tag read or write operations from being performed and prevent some user interface operations. Once the backup is completed, new requests will operate normally. To minimize the potential impact on the automation system, the backup operation should be performed when the system is in an idle state.
- The OPC UA certificates, MQTT certificates, and DA client remote access cannot be backed up.
The backup operation cannot include:
- Incoming and outgoing certificates ofFactoryTalk Linx Gateway
- Trusted and rejected lists
- DA Access option
- The list of approved users that can manage certificates
Refer to Restore
FactoryTalk Linx Gateway
configuration to find steps to restore FactoryTalk Linx Gateway
configuration on
the local computer and distributed data servers.Prerequisites
- Identify the security permissions needed to perform the backup operation. Backup is only available when you have the access in FactoryTalk Security (System>Policies>System Policies>User Rights Assignment>Backup and Restore).
To back up
FactoryTalk Linx Gateway
configuration - In FactoryTalk Administration ConsoleExplorer, right-click theNetworkorLocal, then selectBackup.
- InSpecify archive name, use the default name or a customized name for the backup file.TIP:We don't recommend changing the default archive name. The default name contains the leading digits of the security authority identifier which allows you to easily identify the archive file associated with a specific directory.
- InSpecify archive location, use the default archive path or customize the path as needed.
- InBackup Contents:
- Select.FactoryTalk Linx GatewayconfigurationTIP:This option is not available if theFactoryTalk Linx Gatewayis not installed or the installedFactoryTalk Linx Gatewayversion is earlier than 6.30.00.
- (optional) Selectto back up the entireFactoryTalk DirectoryconfigurationFactoryTalk Directory.
- (optional) Selectto back up theFactoryTalk LinxconfigurationFactoryTalk Linxshortcut and driver configurations.
- To encrypt your archive file, select theEncrypt file contentscheckbox, and then enter the same passphrase in thePassphraseandConfirm passphraseboxes. If you clear this check box, your backup archive file will not be encrypted or protected.Encrypt file contents is not available if your operating system does not support the proper level of encryption.
- SelectOK.
Provide Feedback