Redundant OPC UA Connectors and UA servers

FactoryTalk Linx OPC UA Connector provides redundancy capabilities, where you can configure a redundant pair of data servers that communicate with OPC UA servers.
Install FactoryTalk Linx OPC UA Connector on different computers configured to operate as a redundant pair. FactoryTalk Linx OPC UA Connector will make simultaneous requests to both OPC UA servers. For more information, see Redundancy in
FactoryTalk Linx OPC UA Connector Help.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal