Redundant FactoryTalk Linx servers

FactoryTalk Linx provides redundancy capabilities, where you can configure a redundant pair of data servers that communicate with one ControlLogix controller or redundant ControlLogix systems.
Install FactoryTalk Linx on different computers configured to operate as a redundant pair. The FactoryTalk Linx software will make simultaneous requests to both FactoryTalk Linx servers. The FactoryTalk Linx software will make simultaneous requests to both FactoryTalk Linx servers. To help achieve continuous data feed to increase system availability with minimal impact to network traffic, configure a set of paths to each ControlLogix redundant controller. For more information, see
FactoryTalk Linx Help
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal