Activate FactoryTalk Linx Gateway

To use FactoryTalk Linx Gateway, obtain an activation file that includes an activation key before setting up the software. If the system fails to detect the activation file, an error is logged to
FactoryTalk Diagnostics
, and the system operates under a grace period.
The activation type determines feature support and the maximum capacity of unique tags that can be added to the
FactoryTalk Linx Gateway
server. Increase this count with additional activations and
FactoryTalk Linx Gateway
servers and obtain an activation file for each
FactoryTalk Linx Gateway
server when using different tag counts or features.
We recommend using a shared concurrent activation, which is locked to an activation server computer, but shared by client computers on the network. See
FactoryTalk Services Platform
Help
for more information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal