Restore the Historian WebTrend database
Restoring the backup file ensures no data loss from the original Historian WebTrend
database. This process will replace all existing data on the target computer and is
irreversible. Therefore, we recommend backing up the database first to ensure data
security.
To restore the Historian WebTrend database
- SelectBack Up and Restore Database(
). - UnderRestore the database, upload the .wtdb file.
- Enter the passphrase when backing up the file.
- SelectRestore.
Provide Feedback