Printing reports

  1. In the Editor’s Hierarchy pane, select the list or item(s) that you want to print.
  2. From the
    File
    menu, click
    Print
    . You could also click the
    Print
    button or press ctrl+p to display the
    Print
    dialog box.
  3. Ensure that the correct printer is selected, and click
    OK
    .
    TIP:
    To configure heading and footer fonts, and add a custom footer to your reports, see Setting report preferences for instructions.
Printing a Range of Reports
Occasionally, you may want to print just certain pages of the report. You can do so by entering the starting and ending page numbers of the section you want printed.
  1. In the Editor’s Hierarchy pane, select the list or item(s) that you want to print.
  2. Click
    Print
    .
  3. In the
    Page Range
    area, click
    Pages
    . Type the page numbers to print in the
    From
    and
    To
    boxes.
  4. Ensure that the correct printer is selected and click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal