Setting report preferences

You can define a footer to print on every page of the report and select the font and color (if your printer supports color printing) for the various sections of the report.
  1. From the
    View
    menu, select
    User Preferences
    . The
    User Preferences
    dialog box opens to the
    General
    tab.
  2. Select the
    Reports
    tab. The default report style for most views is
    Formatted
    .
    FTBMM_UserPrefs_Reports Tab
    The
    Reports
    tab contains the following items:
    Item
    Description
    Report
    column
    Lists the report templates available for the item or view that is currently active in the Editor.
    List
    check box
    Enables the list report style, if available for the associated report.
    Formatted
    check box
    Enables the formatted report style, which is the default format for most reports.
    Include Related Data
    check box
    Adds any additional data associated with the selected item to the printed report.
    Footer Text
    Prints the word or phrase entered at the bottom of each report page.
    List Reports
    button
    Formatted Reports
    button
    Opens the
    Report Page Configuration
    dialog box where you can set the margins, font, and text color for a specific report template.
    Graphical Reports
    button
    Not enabled in
    Material Manager
    .
  3. To change the type of printed report, select either
    List
    or
    Formatted
    to the right of the appropriate report.
    TIP:
    If you select the
    List
    format, set the page orientation to landscape. From the
    File
    menu, select
    Print Setup
    , select
    Landscape
    in the Orientation area, and then click
    OK
    .
  4. Where available, you can select
    Include Related Data
    , and any additional data associated with the selected item (single items only – not lists or groups) also prints on the report.
  5. In the
    Footer Text
    box, type a word or phrase to appear centered at the bottom of each page.
  6. Click
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal