Editing storage locations
- In either the Hierarchy or Detail pane, right-click a storage location, and then selectProperties. TheEdit Material Storage Locationdialog box opens to theGeneraltab.
- Make any necessary changes to the general information, and then clickApply.
- Select theMaterialstab. The materials assigned to this storage location display.To make any changes to the list of configured materials, you need to edit the storage container located in the storage location. (See Editing storage containers for more information.)
- To view material properties, double-click a material. TheView Materialdialog box opens.You only can view the material’s property values. To edit the values, use theEdit Materialdialog box. (See Creating a material record for more information.)
- ClickCloseto close the dialog box.
Provide Feedback