Editing storage containers
- In either the Hierarchy or Detail pane, right-click a container, and then selectProperties. TheEdit Material Storage Containerdialog box opens to theGeneraltab. The container name displays in the title bar.
- Make the necessary changes to the storage container.IMPORTANT:If you are changing a value that contains a decimal, use the Delete key to delete the value before typing a new value that contains a decimal. If you type over the old value containing the decimal, the new decimal is not recognized by the application.
- ClickOKto save the changes.
Provide Feedback