Deleting storage locations

  1. To delete a location, right-click on a location and select
    Delete
    .
  2. If
    Confirm deletion
    is enabled on the
    User Preferences
    dialog box, a confirmation message about the selected location opens. To delete the location, click
    Yes
    .
    If
    Confirm deletion
    is disabled on the
    User Preferences
    dialog box, the storage location is deleted without a confirmation message. (See Configuring the Material Editor for more information on defining the user preferences.)
    TIP:
    You cannot delete a material storage location that has material storage containers assigned to it. You must either reassign or delete the containers, and then you can delete the storage location.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal