Editing material properties

  1. If the
    Edit Material
    dialog box is open, select the
    Properties
    tab.
    If not, right-click on a material in the
    Hierarchy
    or
    Detail
    pane, and select
    Properties
    . The
    Edit Material
    dialog box opens. Select the
    Properties
    tab. The currently defined material properties display in a table format. You can also use a form to make changes.
    FTBMM_ED_odin_edit_material_properties_new_2
    For inherited material class properties, you can change only the minimum, maximum, and default values.
  2. Modify the material property as desired.
    IMPORTANT:
    If you are changing a value that contains a decimal, use the Delete key to delete the value before typing a new value that contains a decimal. If you type over the old value containing the decimal, the new decimal is not recognized by the application.
  3. Click
    Apply
    to save the changes, or click
    OK
    to save the record and close the dialog box.
    TIP:
    Changing a duplicate property that is assigned to other materials does not affect the other properties.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal