Creating material types
- From theEditmenu, selectMaterial Types. TheMaterial Typesdialog box opens.
- Click theAddbutton. TheEdit Material Typedialog box opens.
- In theNamebox, type a unique name for the selected material.
- In theDescriptionbox, type a detailed description of the selected material.
- TheController IDfield defaults to the next numeric value in sequence. If necessary, you can change this to a unique number, which is used for PCD phase programming. (See thefor more information.)FactoryTalk BatchPCD Programming Reference Guide
- ClickOKto save the new material type.
Provide Feedback