Configuring material types

A material type is the descriptive state of a material. The
Material Manager
has three default material types:
  • Finished
    is a process output (final product such as vanilla ice cream), which is the quantity of a material that is distributed after the execution of a recipe.
  • Raw
    is a process input, which is the quantity of material, such as milk or eggs, added for the execution of a recipe.
  • Intermediate
    can be both a process input or a process output.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal