Deleting material class properties
- From theMaterial Classesdialog box, select the class, and then click theEditbutton. TheEdit Material Classdialog box opens.
- Select thePropertiestab.
- Select the record row to delete, and then click theDelete Propertybutton.
- ClickApplyto save the changes, or clickOKto save the record and close the dialog box.
Provide Feedback