Migrate configuration from BootP-DHCP Tool
The BootP-DHCP Tool and EtherNet/IP Address Commissioning Tool both will be installed with FactoryTalk Linx by default. However, the tools cannot be used at the same time because of port limitations.
The EtherNet/IP Address Commissioning Tool possesses all the functionalities of BootP-DHCP Tool. The configured relation list in BootP-DHCP Tool can be migrated to EtherNet/IP Address Commissioning Tool.
To migrate configuration from BootP-DHCP Tool
- From the WindowsStartmenu, selectBootP-DHCP Tool.
- Go toFileand selectSaveasto save the current address relation list to a CSV file.
- Close theBootP-DHCP Tool.
- From the WindowsStartmenu, selectEtherNet/IP Address Commissioning Tool.
- On theConfigurationpage, selectImportand find the CSV file just saved.
- SelectOpen.
- (optional) Check the result in theOperation Resultwindow.
Provide Feedback