Manually assign IP
With
EtherNet/IP Address Commissioning Tool
, you can create and maintain a configuration list, that is evaluated when a device provides its MAC address when making a BOOTP/DHCP address assignment request.Manually input the IP address and MAC address for a device using the
Configuration
tab.Prerequisites
- Select a Network Interface Card (NIC).
- Complete the Network information on theSettingstab.
To manually assign IP address for a device
- From theEtherNet/IP Address Commissioning Tool, clickConfiguration.
- ClickAdd, enter all the information in theAdd Itemdialog box, and then clickYes.TIP:To use theCommission from listfunction of the tool, leave the MAC address box empty.
- ClickYesto complete the IP assignment.
Provide Feedback