Number of connections attempted
Description
This is the number of TCP connections that
FactoryTalk Linx
has attempted to initiate, including both those that are currently open and those that have since been closed.Note that for outgoing TCP connections, if no activity occurs on a TCP connection for five minutes, the TCP connection is closed and the diagnostic node for the IP address is removed. This effectively clears the diagnostics counters. When activity resumes on the TCP connection, the diagnostic node is created again. Therefore, these counters provide diagnostics only for the current active "session."
Provide Feedback