Ethernet driver diagnostics counters
Counters related to the Ethernet driver
- Connection state
- IP Address
- Number of connections accepted
- Number of connections active
- Number of connections attempted
- Number of connections closed
- Number of failed connection attempts
- Number of packets in send queue
- Number of packets received
- Number of packets sent
- Number of send failures
- Number of successful connection attempts
- Peak size of send queue
- Port
- Time of last connection establishment
- Time of last connection failure
Provide Feedback