ASync Write calls

Description
This counter indicates the number of requests the OPC DA client made to edit data asynchronously.
The client does not wait for the server to provide an immediate response. Instead, the client continues with its tasks while the server asynchronously notifies the client once obtaining the requested data. This method allows the client to perform other operations without being blocked by the write request.
TIP:
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC DA Server > DaClient_
    X
Value
  • Type: Unsigned integer
  • Source: This value is generated by the FactoryTalk Linx Gateway OPC DA server.
  • Updates: This value increases when an OPC DA client requests to edit data asynchronously.
  • Reset: This value resets when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal