ASync Read Complete calls

Description
This counter indicates the number of completions of asynchronous read operations.
TIP:
Location
  • FactoryTalk Diagnostics Counter Monitor > System Diagnostics > localhost > FactoryTalk Linx Gateway OPC DA Server > DaClient_
    X
Value
  • Type: Unsigned integer
  • Source: This value is generated by the FactoryTalk Linx Gateway OPC DA server.
  • Updates: This value increases when the OPC DA server completes an OPC DA client’s asynchronous read operation.
  • Reset: This value resets when you reset the service or restart the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal