FactoryTalk Live Data diagnostics counters
The following internal counters are made available by
FactoryTalk Live Data
for diagnostic purposes. These counters are supported by FactoryTalk Diagnostics Counter Monitor
.The following counters are available in RnaDaClt side:
The following counters are available in RnaDaSvr side:
Provide Feedback