Min Packet Response Time
Description
The shortest amount of time it has taken
FactoryTalk Linx
to process an unsolicited alarm packet out of the last 100 packets received from the target controller.Data Type
VT_R4
Provide Feedback