Alarm Keep Alive Packets Received
Description
Number of 0 length packets received from the
Logix 5000
controller. Useful for diagnosing whether or not the connection is still open.Data Type
VT_UI4
Provide Feedback