Pending Conditional Events
Description
Size of a queue that holds alarm packets that are received from the controller before we have published the alarm to the
FactoryTalk Alarms and Events
server. Alarms must be published before state changes can be sent.Data Type
VT_UI4
Provide Feedback