Alarm Input-Subscription Max Connections
Description
Shows whether or not a notify object failed to be created because there are already 16 subscribers to this controller.
Data Type
VT_BOOL
Provide Feedback