Pending Conditional Events

Description
The size of a queue that holds alarm packets that are received from the controller before FactoryTalk Linx has published the alarm to the FactoryTalk Alarms and Events server. Alarms must be published before state changes can be sent.
Data Type
VT_UI4
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal