Troubleshooting Resources tab
The
FactoryTalk Diagnostics Counter Monitor
help is integrated into FactoryTalk Diagnostics Counter Monitor
via the Troubleshooting Resources
tab in the Viewer
area. This allows you to view help topics, such as counter descriptions or troubleshooting procedures, on the same screen as the counter data.Click a workstation to show general
FactoryTalk Diagnostics Counter Monitor
help. Click a provider or its children to show the help topic specific to that provider.
Provide Feedback