Data area
The Data area shows the diagnostics counters associated with the target selected in the Navigator area on
FactoryTalk Diagnostics Counter Monitor
main window. The counter values shown are automatically updated every two seconds.The Data area contains the following columns:
- Name: At the root, provider, and client levels, this is the name of the diagnostic counter. At the group level, this is the tag name.
- Value: At the root and provider levels, this is returned data value of the diagnostic counter. At the group level, this indicates the status of the tag: Active or Inactive.TIP:Neither the list of names nor their values can be modified.
Provide Feedback