Points view

Use the
Points
view to configure the device at the individual point level.
Use the
Points
view to:
  • Enable data transmission when an input point changes state.
  • If supported, enable detection of an open circuit in the wiring.
  • If supported, enable detection of loss of field power to the digital input device.
  • If supported, enable latching of diagnostic members so that they remain set after they are triggered.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal