Enable diagnostics for open circuit detection
Enable open circuit detection for each point on the device. An open circuit can be off a terminal, off the load, or a broken wire.
Prerequisites
- Make sure that the connection is configured for Data.
To enable diagnostics for open circuit detection
- On the tab for the device, selectPoints.
- In thePointsview, in theEnable Diagnostics for Open Wirecolumn, select the checkbox for each point to enable open circuit detection.TIP:Select or clear all checkboxes in a column at once by selecting or clearing the checkbox in the header of each column.
- SelectOKto save the changes.
Provide Feedback