Failed to create EtherNet/IP file

Failed to create EtherNet/IP file

The EtherNet/IP file not created.
An error occurred while creating either the folder or file. Refer to the message box for the exact cause of the error.
If this problem continues, create the file manually using RSNetWorx for EtherNet/IP.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal