View trace statistics (XY Plot)
XY Plot calculates statistics (including
averages and time weighted averages) on the data being plotted on the graph.
Statistics calculations are performed on the data for each time period or across
all time periods.
The actual data used as the source for the statistics calculation displays in the
Trace Data
dialog box.To view trace statistics
- On the XY Plot toolbar, clickStatistics
. - In theStatistics, in theCalculate statisticslist, select a time period to view.
- Click one of the following:
- Print Previewto preview the list before sending it to the printer.
- Printto print the list.
- Saveto save the list to a comma or tab delimited file.
Provide Feedback